earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 工程
产品版本: 1.9, 2.0, 2.1, 3.0, 3.1
2020/9/29

Importing a PCT Project

You import a PCT project from your hard drive to use a beforehand saved project.

显示更多
action_close

You import a PCT project from your hard drive to use a beforehand saved project. You export a PCT project to your hard drive to keep a copy of the project at your hard drive.

有关更多信息,请参阅 Importing a PCT Project .

有关更多信息,请参阅 Exporting a PCT Project .

To import a PCT project
  1. In Project Configuration Tool , select the Project view.

  2. On the Header toolbar, select the Import project button

     
    action_zoom_plus_stroke
    .

  3. In the Import Project window, select to the project file you want to import.

  4. Click Open .

  5. In the Import project dialog box, in the Project name box, type the name of your project.

    • Select Create as new to create a new project.

    • Select Replace '[project's name]' to override the previous version of this project.

    注释:

    When importing the project, a name conflict can be resolved in either creating a new project or replacing a previous version of the imported one. The project name is encoded in the file metadata.

    If you see the message "Project name already used", you need to type a new project name, which is different from each of the existing project names.

  • Import and Export a PCT Project
  • Project Configuration Tool Projects
  • Project Configuration Tool Client
  • Import Project Dialog Box
  • Exporting a PCT Project