earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
1
概念

概念


产品: RP-C, RP-C-EXT-IS-BLE
功能: 硬件
产品版本: 2022, 2023
2022/4/5

People Counting

The Insight-Sensor supports people counting through a thermal image sensor.

 
action_zoom_plus_stroke Thermal Image Sensor
图: Thermal Image Sensor

The sensor is designed to detect and count people in an area inside a building. The people counting function can be used, for example, for space (occupancy) management and control of HVAC.

Based on innovative image processing and thermal infrared imager technology, the sensor detects people and counts anonymously each person in a specific area.

The thermal image sensor is of type longwave infrared (LWIR) microbolometer, without any mechanical shutter. The sensor has a wide field of view of 120 degrees. The sensor is light-independent and works even in total darkness. The thermal images captured by the sensor are of low resolution (80 x 80 pixels).

The thermal image sensor senses the heat radiation from each individual. The device applies advanced image processing to the thermal images, and the result is a people count number, which is periodically transmitted to the RP controller. The information from the device cannot be used to identify people.

 
action_zoom_plus_stroke Example of a thermal image of 11 people sitting around a table
图: Example of a thermal image of 11 people sitting around a table

To enable the people count calculations, the thermal image captured by the sensor is compared to a background image. The background image is an image without any people present in the area. The background image can be refreshed by executing a command in the EcoStruxure Building Operation software. The command can be executed either automatically, once a day at a configurable time, or manually. Depending on the configuration, the background image is not refreshed (captured) immediately, but only when the passive infrared (PIR) sensor indicates that no one has moved in the area recently, for example, the last 10 minutes. 有关更多信息,请参阅 Segment People Count Inputs .

The Insight-Sensor must be installed with the thermal image sensor facing down. If the device is installed on a wall, the thermal image sensor will not work properly.

通知

REDUCED DEVICE PERFORMANCE

  • Always install the device with the thermal image sensor facing down.

  • Ensure that the device is not tilted.

Failure to follow these instructions can result in reduced device performance.

The Insight-Sensor supports mounting heights from 2.5 to 3 m (8.2 to 10 ft). Installing the device higher than 3 m (10 ft) or lower than 2.5 m (8.2 ft) from the floor can significantly impair the performance of the people counting function. The height at which the device is installed must be configured in the EcoStruxure Building Operation software during commissioning. If the installed height is not correctly configured in the software, the counting accuracy may be degraded. 有关更多信息,请参阅 Configuring an Insight-Sensor .

通知

REDUCED DEVICE PERFORMANCE

  • Do not install the device higher than 3 m (10 ft) or lower than 2.5 m (8.2 ft) from the floor.

  • In the EcoStruxure Building Operation software, configure the height at which the device is installed.

Failure to follow these instructions can result in reduced device performance.

The sensor detection range depends on which height the sensor is mounted, as shown in the following figure and table. The detection range is measured at the level of 1 m (3.3 ft) above the floor.

 
action_zoom_plus_stroke People counting detection range (diameter)
图: People counting detection range (diameter)

Sensor mounting height

Sensor detection range (diameter)

3.0 m (10 ft)

7.0 m (22 ft)

2.7 m (9 ft)

5.8 m (19 ft)

2.5 m (8 ft)

5.2 m (17 ft)

The accuracy of the people counting function is specified below. The value specified is an average and not the accuracy of each measurement. As described, the counting accuracy depends on several different conditions that must be met.

Average counting accuracy

Conditions

Up to 90%

The conditions that must be met to achieve the specified counting accuracy primarily include, but is not limited to, a correctly installed and configured device.

Examples of additional conditions that affect the counting accuracy and therefore need to be considered:

  • More than 50% of the person needs to be visible for the sensor to be able to count the person.

  • The temperature of floors and walls in people's immediate vicinity can affect the counting accuracy if the temperature is in the same range as the human body temperature.

  • The presence of windows heated by solar rays, radiators, and other large objects with a temperature in the same range as the human body temperature can affect the counting accuracy. The impact of such objects can be reduced by using masks. 有关更多信息,请参阅 Insight-Sensor Masks .

The sensor itself does not need to be calibrated on site, but as mentioned above, the installed height must be configured in the EcoStruxure Building Operation software during commissioning. Depending on the installation, the properties for refresh of the background image as well as the sensor's detection area may need to be configured.

The EcoStruxure Building Operation software provides the following Insight-Sensor configuration properties:

  • Installed height (distance from the floor to the device in the ceiling)

  • Refresh background mode (automatic or manual)

  • Refresh background time (time of day when the command for automatic refresh of the background image is triggered)

  • Minimum no motion time (minimum time without any motion detected that must elapse before the refresh background command is executed)

有关更多信息,请参阅 Configuring an Insight-Sensor .

Using the EcoStruxure Building Operation software, the thermal image sensor's detection area can be configured to reduce overlapping areas between two devices to minimize the risk of a person being counted twice. The detection area can also be adjusted to exclude heat radiating objects such as radiators and windows heated by solar rays, and to exclude corridors and other adjacent areas through which people just pass by.

有关更多信息,请参阅 Insight-Sensor Masks .

  • RP Controller Expansion Modules
  • Sensor Modules
  • RP-C-EXT-IS-BLE
  • Segment People Count Inputs
  • Insight-Sensor Masks
  • Configuring an Insight-Sensor
  • Motion Detection
  • RP Controller Expansion Insight-Sensor Device Installation