earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Dashboards
Product version: 2022, 2023
2/23/2024

Alarm Pareto Chart Dialog Box

Use the Alarm Pareto Chart dialog box to configure and edit an alarm Pareto chart.

 
action_zoom_plus_stroke Alarm Pareto Chart - dialog box
Figure: Alarm Pareto Chart - dialog box

Table: Alarm Pareto Chart Dialog Box

Component

Description

Column

Select the column(s) you want to display in the widget.

Filter

Select the filter you want to apply.

Max number of bars

Enter the number of bars you want to display in the chart.

Caption

Type a caption for the widget.

Caption Link

Select to make a link to an object that is relevant to the values that are displayed in the widget.

Show Legend

Click True to display the name and color of the trend log in the widget.

Show Period

Select to display the period as a legend.

Bar color

Select the color you want to use on the bars.

Y-axis minimum

Enter the Y-axis minimum.

Y-axis maximum

Enter the Y-axis maximum.

Y-axis

Select the position of the y-axis.

Decimals

Select the number of decimals you want to display.

  • How Dashboards Work
  • Dashboard Widgets
  • Widget Dialog Box – Layout Tab