Use the Alarm Pie dialog box to configure and edit an alarm pie.
Component |
Description |
Column |
Select the column(s) you want to display in the widget. |
Filter |
Select the filter you want to apply. |
Max number of slices |
Select the number of slices you want to display in the pie chart. |
Color |
Select the color for the trend log. |
Period |
Select the period you want to display. |
Caption |
Type a caption for the widget. |
Caption Link |
Select to make a link to an object that is relevant to the values that are displayed in the widget. |
Pie Center |
Select how you want to display the pie center. For more information, see Log Pie . |
Show Legend |
Click True to display the name and color of the trend log in the widget. |
Show Percentage |
Select to display the values in percentage. |
Display Value |
Select to display the alarm states as legends in the slices. |
Decimals |
Select the number of decimals you want to display. |