Use the Alarm Sankey Chart dialog box to configure and edit an alarm Sankey chart.
Component |
Description |
Column |
Select the column(s) you want to display in the widget. |
Filter |
Select the filter you want to apply. |
Max number of nodes |
Enter the number of bars you want to display in the chart. |
Caption |
Type a caption for the widget. |
Caption Link |
Select to make a link to an object that is relevant to the values that are displayed in the widget. |
Show Legend |
Click True to display the name and color of the trend log in the widget. |
Decimals |
Select the number of decimals you want to display. |