earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 3.2, 3.3, 2022
3/10/2021

Syntax for IP Address Allow List

You configure the Allow list to allow access only from specific IP addresses or from ranges of IP addresses. If nothing is configured, then all IP addresses are allowed.

You can use two different syntax for lists of IP addresses:

  • A list of line separated IP addresses:

    192.168.0.1

    127.0.0.1

  • A range of IP addresses in CIDR notation on one or many lines:

    10.0.0.0/8

    10.0.0.0/16

You can also use a combination of both.

Note:

EcoStruxure BMS does not accept other syntax for specifying IP range, eg. 10.0.0.0 - 10.0.0.255

  • Windows Active Directory User Groups
  • User Account Group – Policies Tab
  • Creating a User Account Group