earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 3.2
3/24/2021

User Account Group – Policies Tab

Use the Policies tab to edit the policy settings for a user account group.

 
action_zoom_plus_stroke Policies tab
Figure: Policies tab

Table: Policies Tab

Component

Description

User Interactivity

Select to let users log off and close WorkStation.

Audit Trailing

Select to enable audit trailing for users belonging to this group.

Password

Select to enable the user account group members to change their passwords.

Web Configuration

Select to enable users to access the Web Configuration where you configure the settings of a SmartX server. For more information, see SmartX Server Device Configuration in WebStation .

Personal Favorites

Select to enable the user account group members to create personal favorites and a personal overview of their system

Personal Dashboards

Select to enable the user account group members to create personal dashboard.

Automatic Logoff

Select to log off users in this group after a defined time of inactivity. For more information, see Automatic Logoff .

Log Off To Guest Account

Select to logoff users in this group to the guest account after a defined time of inactivity. For more information, see Automatic Logoff to Guest Account .

IP Address Allow list

Type the list of IP addresses that are allowed for the group members to log on from. For more information, see Syntax for IP Address Allow List .

Activation Schedule

Browse to the multistate schedule regulating the user account group members access hours.

Schedule Value When Active

Enter the value the schedule has when it is active.

Zoning

Select to allow the user account group members to perform zoning actions.

Change Control

Select to enable user account group members to add comments and sign changes made in the system.

User Settings

Select to enable user account group members to display invalid objects in WorkStation.

  • Software Permissions, User Accounts, and User Account Groups
  • User Account Group Wizard – Windows Group Name and Group Policies Page
  • SmartX Server Device Configuration in WebStation
  • Automatic Logoff
  • Automatic Logoff to Guest Account
  • Syntax for IP Address Allow List
  • Select Object and Property Dialog Box