earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 2022, 2023
2021-12-17

Adding or Changing a Unit and Prefix for a Value in WebStation

You define and change the unit and its prefix for a value to ensure that the value is correct calculated.

Pokaż więcej
action_close

You add objects to the Watch pane to monitor their live values.

For example, you can monitor the impact of a change you are about to make in your system. Property changes are immediately displayed in the Watch pane.

You can save the Watch pane with all its objects and properties so that you can use it again the next time you log on to WebStation.

To add or change a unit and prefix for a Value in WebStation
  1. In WebStation, open the properties dialog box for the object with the value you want to change unit and prefix on.

  2. Click the Context menu button

     
    action_zoom_plus_stroke
    for the value.

  3. Click Configure unit .

  4. Select the unit and prefix.

  5. Click OK .

  • Modify Values
  • Value Presentation