earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: WorkStation, WebStation
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 2022, 2023
2021-12-17

Modify Values

arrow1_rotationForced Values arrow1_rotationAdd and Change Units and Prefix

You can change and force values using a graphic or the Properties pane. Using the Watch pane, you can dynamically monitor a value.

Forced Values

When you force a value, all input from the system is overridden. For example, a schedule is set to start a fan at 09:00 but you want it to start at 08:00. In this case, you can force the fan to start at 08:00.

Więcej informacji zawiera Forced Values .

Add and Change Units and Prefix

You can add or change units and prefixes on values using WebStation.

Więcej informacji zawiera Adding or Changing a Unit and Prefix for a Value in WebStation .

  • WorkStation Overview
  • WebStation Overview
  • Value Presentation
  • Forced Values
  • Watch Pane and Watch View
  • Watch Pane and Watch View Toolbar
  • Graphics Toolbar
  • Adding an Object to the Watch Pane or a Watch View
  • Removing an Object from the Watch Pane or a Watch View
  • Changing a Value in a Graphic