Use Search to find and view objects in the EcoStruxure BMS database.
Different Searches
There are two different ways to search in WebStation:
The Search function searches for all object names and property names in the system.
A saved search is a predefined search that searches specific criteria in a specific part of the system. Saved searches are created in WorkStation and the search criteria cannot be changed in WebStation.
Search is case insensitive, which means that Search does not distinguish between uppercase and lowercase letters. A search for "Fan" results with hits for both "fan" and "Fan".
Wildcards
Use wildcards to substitute characters or combinations of characters in a search.
Search supports two main wildcards:
For example, you want to find all objects and properties containing the word “Temperature”. You start the search with an asterisk so that the search includes all hits on objects like “Outside Air Temperature” where the asterisk represents the words before "Temperature", in this case “Outside Air”. You also have to end the search text with an asterisk to include objects like “Temperature Alarm” where the asterisk represents the word after "Temperature", in this case “Alarm”.
Local or Global Searches
You can search in your whole EcoStruxure BMS or only in a folder, device, or server:
To search your whole system, select the top server and then perform the search. You can also click the Search whole server button in the list.
To search a specific folder, select the folder and then perform the search.
Uwaga
When you perform a search, you cannot leave the Search box empty. To perform a search, you have to enter something in the Search box.
Export a search
You can export a search result as an Excel file.
Multi-edit in the search list view
You can multi-edit several objects in the search result list at the same time. This saves a lot of time compared to editing the objects one by one.
Więcej informacji zawiera Multi-editing in Search
.