Produits : WebStation
Fonctionnalités : Calendriers
Version produit : 2024, 7.0
03/12/2024

Creating a Multi Schedule Viewer

You create a Multi schedule viewer to view and edit several schedules at the same time.

Afficher plus
action_close

You can create a Multi schedule viewer in WebStation to edit and view a number of schedules at the same time.

A Multi schedule viewer is useful for example if you want to add at the same events on several schedules at the same time. You can select the schedules you want to add the events on.

A Multi schedule viewer also gives you an overview of the attached schedules.

To create a Multi schedule viewer
  1. In WebStation, in the System Tree pane, right-click a schedule you want to include in the Multi schedule viewer and click Create Multi schedule viewer .

  2. In the Name field, type a name.

  3. In the Path field, enter the location of the Multi schedule viewer.

  4. Click Add to add more schedules to the Multi schedule viewer.

  5. In the Select object dialog box, do one of the following:

    • Click Browse to browse the system to find the schedules you want to add.

    • Click Object matching type , to get a list of all schedules in the system that can be added.

  6. Select the schedules you want to add.

  7. Click Select .

  8. Click OK .

Déclaration

You can also add new schedules to the Multi schedule viewer by clicking the Add button in the Multi schedule viewer toolbar. Pour plus d'informations, voir Adding a Schedule to a Multi Schedule Viewer .

  • Multi Schedule Viewer
  • Multi Schedule Viewer Workspace
  • Multi Schedule Viewer Toolbar
  • Adding a Schedule to a Multi Schedule Viewer
  • Removing a Schedule from a Multi Schedule Viewer
  • Adding the Same Event to Multiple Schedules
  • Assigning a Value on Click
  • Opening a Schedule from a Multi Schedule Viewer