Produits : WebStation
Fonctionnalités : Calendriers
Version produit : 2024, 7.0
03/12/2024

Adding a Schedule to a Multi Schedule Viewer

You add schedules to a Multi schedule viewer to get an overview and be able to edit several events from the same Multi schedule viewer.

Afficher plus
action_close

You can create a Multi schedule viewer in WebStation to edit and view a number of schedules at the same time.

A Multi schedule viewer is useful for example if you want to add at the same events on several schedules at the same time. You can select the schedules you want to add the events on.

A Multi schedule viewer also gives you an overview of the attached schedules.

To add a schedule to a multi schedule viewer
  1. In WebStation, click the Multi schedule viewer.

  2. In the Multi Schedule Viewer toolbar, click the Add button

     
    action_zoom_plus_stroke
    .

  3. In the Select object dialog box, do one of the following:

    • Click Browse to browse the system to find the the schedules you want to add.

    • Click Object matching type , to get a list of all schedules in the system that can be added.

  4. Select the schedules you want to add.

  5. Click Select .

  6. Click Save .

  • Multi Schedule Viewer
  • Multi Schedule Viewer Workspace
  • Multi Schedule Viewer Toolbar
  • Creating a Multi Schedule Viewer
  • Removing a Schedule from a Multi Schedule Viewer
  • Adding the Same Event to Multiple Schedules
  • Assigning a Value on Click
  • Opening a Schedule from a Multi Schedule Viewer