earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Schedules
Product version: 2022, 2023
12/17/2021

Adding the Same Event to Multiple Schedules

You add the same event on multiple schedules in the Multi schedule viewer to save time.

Show More
action_close

You can create a Multi schedule viewer in WebStation to edit and view a number of schedules at the same time.

A Multi schedule viewer is useful for example if you want to add at the same events on several schedules at the same time. You can select the schedules you want to add the events on.

A Multi schedule viewer also gives you an overview of the attached schedules.

To add the same event to multiple schedules
  1. In WebStation, in the Multi schedule view, select the schedules that you want to add the event on.

  2. Drag over the schedule to add the event on the schedule.

  3. Click Save .

  • Multi Schedule Viewer
  • Multi Schedule Viewer Workspace
  • Multi Schedule Viewer Toolbar
  • Creating a Multi Schedule Viewer
  • Adding a Schedule to a Multi Schedule Viewer
  • Removing a Schedule from a Multi Schedule Viewer
  • Assigning a Value on Click
  • Opening a Schedule from a Multi Schedule Viewer