earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: RP-V
Funkcje: Sprzęt
Wersja produktu: 2022, 2023, 2024, 7.0
2023-03-30

RP-V Screw Terminals

arrow1_rotationRP-V-4A Screw Terminals arrow1_rotationRP-V-5A Screw Terminals arrow1_rotationRP-V-5C-M Screw Terminals

The RP-V has fixed screw terminals for the power input, SSR outputs, and universal inputs/outputs. The RP-V-5C-M model also has a removable screw terminal block for connection to the BACnet MS/TP (RS-485) network.

The wiring recommendations are provided separately. Więcej informacji zawiera Wiring .

RP-V-4A Screw Terminals

The RP-V-4A model has four I/O points and the controller is equipped with 11 fixed screw terminals.

Więcej informacji zawiera RP-V-4A Screw Terminals .

RP-V-5A Screw Terminals

The RP-V-5A model has five I/O points and the controller is equipped with 11 fixed screw terminals.

Więcej informacji zawiera RP-V-5A Screw Terminals .

RP-V-5C-M Screw Terminals

The RP-V-5C-M model has five I/O points and the controller is equipped with 11 fixed screw terminals and a 3-position removable screw terminal block.

Więcej informacji zawiera RP-V-5C-M Screw Terminals .

  • RP-V Controllers
  • RP-V Models
  • RP-V-4A Screw Terminals
  • RP-V-5A Screw Terminals
  • RP-V-5C-M Screw Terminals
  • Wiring