Produkty: Operator Display
Funkcje: Harmonogramy
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Schedule Detail Screen

Use the schedule detail screen to view the detailed properties of the schedule.

 
action_zoom_plus_stroke Schedule detail screen
Rysunek: Schedule detail screen

Tabela: Schedule Detail Screen

Component

Description

Name

Displays the name of the schedule.

Description

Displays the description of the schedule.

Present value

Displays the current schedule output value. Więcej informacji zawiera Schedule Events .

Default value

Displays the schedule default value. Więcej informacji zawiera Schedule Events .

Effective Period

Displays the range of time the schedule is in service. Więcej informacji zawiera Schedule Events .

Priority for writing

Displays the priority at which the referenced properties are commanded. Więcej informacji zawiera BACnet Command Priorities .

  • Schedule Handling
  • Exception Event Priorities
  • Schedule Events
  • BACnet Command Priorities
  • Schedules Screen