earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: Operator Display
Funkcje: Harmonogramy
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Multi-State/Enumerated Schedules

A multi-state or enumerated schedule controls objects that have states based on integers or positive whole numbers including zero.

For example, a multi-state weekly schedule is bound to a multi-state value that controls an air handling unit in an office building. It regulates the air circulation Monday through Friday from 08:00 to 17:00, to 2 (occupied) when the schedule is active and 1 (unoccupied) when the schedule is inactive.

 
action_zoom_plus_stroke Multi-state schedule
Rysunek: Multi-state schedule
  • Schedule Types
  • Weekly Events
  • Adding a Weekly Event
  • Editing a Weekly Event