earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Schedules
Product version: 3.3, 2022, 2023, 2024
7/22/2021

Edit Exception Event Screen

Use the Edit exception event screen to add, edit or delete the time and value of an exception event.

 
action_zoom_plus_stroke Edit exception event screen
Figure: Edit exception event screen

Table: Edit Exception Event Screen

Component

Description

Value type

Displays the schedule type the event is added to. For more information, see Schedule Types .

Value

Tap - or + to edit the schedule output value when this event is active. For more information, see Weekly Events .

This field will be different if you have selected to edit a digital schedule event.

All day

Tap All day to make the event span 24 hours instead of selecting specific hours using From and To .

From

Tap - or + to edit the starting time of the event.

To

Tap - or + to edit the ending time of the event.

  • Schedule Handling
  • Weekly Events
  • Exception Events
  • Schedules Screen