earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: BACnet/IP devices
Product version: 3.3, 2022, 2023, 2024
7/22/2021

Device Info Screen

Use the device info screen to view more information on the device and rediscover to refresh its inputs, outputs, and values.

 
action_zoom_plus_stroke Device info screen
Figure: Device info screen

Table: Device Info Screen

Component

Description

Name

Displays the device name.

Description

Displays the device description.

Object ID

Displays the BACnet device identification number.

Firmware version

Displays the device firmware version number.

Serial number

Displays the device serial number.

IP address

Displays the IP address.

Model

Displays the device model number.

Vendor

Displays the device vendor name.

Vendor ID

Displays the device vendor identification number.

Rediscover

Tap to refresh the device inputs, outputs, and values.

  • Configuration