earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: Operator Display
Funkcje: Harmonogramy
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

Analog Schedules

An analog schedule controls objects with real numbers. The real numbers include positive or negative numbers, fractions, and decimal values.

For example, an analog schedule regulates a thermostat setpoint in an office area. It controls the temperature from 08:00 to 17:00, to 22 °C (72 °F) when the schedule is active and 16 °C (62 °F) when the schedule is inactive.

 
action_zoom_plus_stroke Analog schedule
Rysunek: Analog schedule
  • Schedule Types
  • Weekly Events
  • Adding a Weekly Event
  • Editing a Weekly Event