earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Alarms
Product version: 3.3, 2022, 2023, 2024, 7.0
7/22/2021

Alarms Screen

Use the Alarms screen to display alarms for all the devices available on this Operator Display.

 
action_zoom_plus_stroke Alarms screen
Figure: Alarms screen

Table: Alarms Screen

Component

Description

Count

Displays the number of times the alarm has been activated before it is acknowledged.

Time

Displays the date and time of the most recent alarm state change.

Device

Displays the name of the device.

Source

Displays the name of the input, output or value that activated the alarm.

Message

Displays the alarm message corresponding to the alarm state. For more information, see Alarm Handling .

 
action_zoom_plus_stroke

Indicates an active alarm in the state Alarm that is not acknowledged. For more information, see Alarm Handling .

 
action_zoom_plus_stroke

Indicates an active alarm in the state Fault that is not acknowledged. For more information, see Alarm Handling .

 
action_zoom_plus_stroke

Indicates an active alarm that is acknowledged. For more information, see Alarm Handling .

 
action_zoom_plus_stroke

Indicates a reset alarm that is not acknowledged. For more information, see Alarm Handling .

 
action_zoom_plus_stroke

Tap to open the alarm detail screen, where you view more information and acknowledge the alarm. For more information, see Alarm Detail Screen .

  • Alarm Handling
  • Alarm Detail Screen