Produkty: Operator Display
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.3, 2022, 2023, 2024, 7.0
2021-07-22

About Screen

Use the About screen to display more information on Operator Display.

 
action_zoom_plus_stroke About screen
Rysunek: About screen

Tabela: About Screen

Component

Description

Model

Displays the Operator Display part number.

Platform version

Displays current platform version number.

Application version

Displays the current firmware version number.

ETH1 MAC address

Displays the MAC address for the Ethernet interface.

BACnet Device Name

Displays the device name defined in the BACnet Setup screen. Więcej informacji zawiera Configuring the BACnet/IP Network Communication .

BACnet Device Description

Displays the device description defined in the BACnet Setup screen. Więcej informacji zawiera Configuring the BACnet/IP Network Communication .

Erase all data

Tap to erase the device list, logs, and users from the Operator Display. The only data remaining will be the firmware version and time setting.

This task requires administrator permissions.

  • Operator Display Overview
  • Hardening Specifics
  • Configuring the BACnet/IP Network Communication