earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P
功能: Semantic
产品版本: 2023
2023/2/28

Uploading Ontologies

You upload ontologies on your system so that the correct ontologies are used on the semantic database.

显示更多
action_close

Semantic is based on ontologies.

When you navigate a semantic database the Sparql queries that are used in navigation are executed on the semantic database. The results are then sent to Enterprise Server or Enterprise Central.

EcoStruxure Building Operation supports Brick ontology version 1.3.

Upload Ontologies

You can at any time upload an ontology from the EBO server to the semantic database. In some occasions you need to upload the ontologies from the Enterprise Server or Enterprise Central to the semantic database. This is done, for example, if you want to restore a semantic database. It is also done if you change the location of your semantic database from the default installation to another computer.

有关更多信息,请参阅 Uploading Ontologies .

Enterprise server and Enterprise Central are delivered with the following ontologies. These are uploaded to the semantic database the first time you upload ontologies.

  • The default graph

  • https://brickschema.org/schema

  • https://w3id.org/se/building/extension

  • https://w3id.org/se/building/nsp

  • https://w3id.org/se/building/project

To upload ontologies
  1. In WorkStation open System .

  2. Right-click Semantic and click Upload ontologies .

  • Semantic Overview
  • Configure EcoStruxure Building Automation System to use Semantic Workflow
  • Configuring the Semantic Settings
  • Ontologies
  • Configuring Semantic Permissions
  • Uploading Ontologies