Log on to rate and give feedback
12345Log on to rate
0
Как
Продукты:
WebStation
Функции:
Расписания
Версия продукта:
2024, 7.0
02.12.2024
Opening a Schedule from a Multi Schedule Viewer
You can open a schedule from a Multi schedule viewer if you want to edit the schedule.
Показать больше
action_close
You can create a Multi schedule viewer in WebStation to edit and view a number of schedules at the same time.
A Multi schedule viewer is useful for example if you want to add at the same events on several schedules at the same time. You can select the schedules you want to add the events on.
A Multi schedule viewer also gives you an overview of the attached schedules.
To open a schedule from a Multi Schedule Viewer
In WebStation, click the Multi schedule viewer.
In the Multi schedule viewer, right-click the name of the schedule you want to edit and click
Open schedule
.