earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Commission, IP-IO , MP-C, MP-V, RP-C, RP-V
Functionalities: Engineering, BACnet/IP devices
Product version: 2024, 7.0
9/11/2024

Logging on to the Commission Mobile Application

You log on to the Commission mobile application to perform commissioning, flow balance, and checkout operations on BACnet/IP controllers.

Show More
action_close

The Commission mobile application allows you to use a mobile device to perform commissioning, flow balance, and checkout operations on SpaceLogic BACnet/IP devices. BACnet/IP devices include BACnet/IP controllers (MP and RP), and IP-IO modules. The Commission mobile application is available for Android and iOS (Apple) phones and tablets, as well as devices using Microsoft Windows. The Commission mobile application can connect to a single BACnet/IP device or to a network of BACnet/IP devices on the local network.

Device Connection

The Commission mobile application supports device connection through BACnet Wi-Fi and wireless Bluetooth connection.

For more information, see Device Connection .

Bluetooth Adapter

The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to SpaceLogic and EasyLogic controllers that contain an extra COM port. You plug the Bluetooth adapter into the corresponding SpaceLogic Sensor to connect to the controller.

For more information, see SpaceLogic Bluetooth Adapter .

Device Configuration

You configure the device settings of a BACnet/IP device so that it can communicate on the network. For example, in the Commission Mobile Application, you can configure the BACnet/IP controller so that it can communicate on the IP network, or configure it as an MS/TP device to enable it to communicate on an MS/TP network.

For more information, see BACnet/IP Controller Device Settings .

Configuration Menu

Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a BACnet/IP controller to commission the controller.

For more information, see Configuration Menu .

I/O Checkout

After you have wired the physical inputs and outputs of the controller, you perform I/O checkout to verify that the wiring was done correctly and that the physical inputs and outputs are working properly.

For more information, see I/O Checkout Overview .

Flow Balancing

The Flow Balance function of the Commission mobile application is used to air balance terminal boxes controlled by VAV controllers. This function automates most of the air balance procedure but it also allows you to manually check out the flow balance by driving the damper to a specified position, a flow setpoint, or a flow value.

For more information, see Flow Balancing .

Device Restart

Use the Device Restart function of the Commission mobile application to perform a restart of the BACnet/IP controller. There are four different ways to restart the BACnet/IP controller.

For more information, see Device Restart .

To log on to the Commission mobile application
  1. Download and then install the Commission mobile application to the mobile device or Windows laptop from Google Play, the Apple App Store, or the Microsoft Store.

    Tip:

    EcoStruxure Building Commission is the name of the application used in the download sources.

  2. From your mobile device or Windows laptop, launch the application by logging on with your Schneider Electric extranet credentials while connected to the internet.

    Important:

    You can use the mobile application indefinitely without an internet connection once you have logged in. If the device is not connected to the Internet, you are unable to log out. This prevents you from accidentally logging out while unconnected to the Internet and supports secure applications where the device running the application is not allowed to connect to the Internet.

    When connected to the Internet, you are required to log out and back in every 90 days to renew your user-credential access token. Seven days prior to the expiration of the 90-day period, you start receiving reminders to log out and back in again to begin a new 90-day period.

    A page then displays with the name of the product, EcoStruxure Building Commission. It is followed by a prompt indicating that by using this product, you accept its Terms of Use .

  3. Click Terms of Use to view the terms and conditions.

  4. Export this information by clicking the Share button and then use the share options available on your device to send the text to the target location of your choice.

  5. Click Close to exit the Terms of Use page and then click Accept and Continue .

    You will not see that Terms of Use prompt next time you log in.

    The logon page displays next and includes the product name and application software version.

  6. Click Log on .

    The logon process has been integrated with Schneider Electric’s identity management system.

  7. On the ensuing EcoStruxure Building Commission page, enter your email address and click Next or click the single sign-on button

     
    action_zoom_plus_stroke
    to continue with your Schneider Electric Exchange account.

    If you do not have a user account, click Register here to register here as a new user and create one.

    Once you have authenticated your user account, the Consent Management page displays and you are prompted to Personalize Your Experience .

  8. Please opt in to allow Schneider Electric to utilize your real-world use case data to improve the mobile application in the future.

    Tip:

    Should you opt in, you can change permission settings at any time by accessing the Consent Management page from the More page. For more information, see Accessing and Using the More Menu .

  9. Click the button

     
    action_zoom_plus_stroke
    to turn on and send analytic events based upon what you are doing in the application.

    If you click to turn it off, you do not send any analytic data.

  10. Click Close to exit and view Home page.

When you launch the Commission mobile application from your mobile device, you will immediately come to the Home page. You do not need to perform the user authentication process unless you logout.

  • Commission Mobile Application
  • Accessing and Using the More Menu