earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Commission, IP-IO , MP-C, MP-V, RP-C
Functionalities: Engineering, BACnet/IP devices
Product version: 2022, 2023, 2024, 7.0, 7.1
2/13/2025

Accessing and Using the More Page

You use the More page to do the following in the Commission mobile application:

  • Access the Web Help and Video help features

  • View the privacy notice, terms of use and about pages

  • Send or stop sending analytic events

  • Log out

Show More
action_close

The Commission mobile application allows you to use a mobile device to perform commissioning, flow balance, and checkout operations on SpaceLogic BACnet/IP devices. BACnet/IP devices include BACnet/IP controllers (MP and RP), and IP-IO modules. The Commission mobile application is available for Android and iOS (Apple) phones and tablets, as well as devices using Microsoft Windows 10. The Commission mobile application can connect to a single BACnet/IP device or to a network of BACnet/IP devices on the local network.

Device Connection

The Commission mobile application supports device connection through BACnet Wi-Fi and wireless Bluetooth connection.

For more information, see Device Connection .

Bluetooth Adapter

The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to MP controllers. You plug the Bluetooth Adapter into the corresponding SpaceLogic Sensor to connect to the controller.

For more information, see SpaceLogic Bluetooth Adapter .

Device Configuration

You download an image to a BACnet/IP controller to facilitate device commissioning tasks and then use the Device Settings view to configure the settings of the BACnet/IP controller.

For more information, see BACnet/IP Controller Device Settings .

Configuration Menu

Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a BACnet/IP controller to commission the controller.

For more information, see Configuration Menu .

I/O Checkout

After you have wired the physical inputs and outputs of the controller, you perform I/O checkout to verify that the wiring was done correctly and that the physical inputs and outputs are working properly.

For more information, see I/O Checkout Overview .

Flow Balancing

The Flow Balance function of the Commission mobile application is used to air balance terminal boxes controlled by MP-V controllers. This function automates most of the air balance procedure but it also allows you to manually check out the flow balance by driving the damper to a specified position, a flow setpoint, or a flow value.

For more information, see Flow Balancing .

Device Restart

Use the Device Restart function of the Commission mobile application to perform a restart of the BACnet/IP controller. There are four different ways to restart the BACnet/IP controller.

For more information, see Device Restart .

To access and use the More page
  1. In the Commission mobile application, on the tab bar, click More .

    The first and last names of the current user are displayed.

  2. Click Settings to change the application language, and access the Operating System settings for the Commission mobile application.

  3. Under Get Support , click to access the help features of the Commission mobile application such as Web Help and Video Help .

  4. Under Permissions & Privacy , click Privacy to see the application’s privacy notice.

  5. Click to access the Consent Management page that you saw previously during the log in process.

    For more information, see Logging on to the Commission Mobile Application .

  6. Click  Consent Management  to opt-in or opt-out of allowing Schneider Electric to collect application usage information.

  7. Click  Terms of Use  to view terms and conditions.

  8. Click  About  to view the application version number.

  9. Click Third Party Acknowledgements to view third-party license information.

  • Commission Mobile Application
  • Logging on to the Commission Mobile Application