earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P
Functionalities: Semantic
Product version: 2024, 7.0
12/2/2024

Semantic View in WebStation

Use Semantic View to navigate the semantic database in WebStation.

 
action_zoom_plus_stroke Semantic view
Figure: Semantic view

Table: Semantic View

Number

Description

 
action_zoom_plus_stroke

Semantic Navigator

Use Semantic Navigator to navigate between related items in the semantic model that describes the building and the installed system.

For more information, see Semantic Navigator in WebStation .

 
action_zoom_plus_stroke

Semantic Breadcrumb

Use Semantic Breadcrumb to navigate between semantic items and to display a semantic items relations.

Use the breadcrumb to ... For more information, see Semantic Breadcrumb .

 
action_zoom_plus_stroke

Semantic Graph View

Use Semantic Graph View to get a graphic overview of the semantic system.

For more information, see Semantic Graph View .

 
action_zoom_plus_stroke

Semantic Information List

Use Semantic Information List to navigate among objects in the semantic database and the connected EcoStruxure Building Operation objects. From the list you can also edit, for example properties on the related EBO objects.

For more information, see Semantic Information List .

  • Semantic Overview
  • Semantic View in WebStation
  • Semantic Navigator in WebStation
  • Semantic Information List
  • Semantic Graph View
  • Semantic Breadcrumb