Produkty: AS-B, Enterprise Central, Enterprise Server, AS-P
Funkcje: Semantic
Wersja produktu: 2022
2022-03-23

Semantic Engineering Context Menu

Use the Semantic engineering menu to edit the semantic model in the Semantic editing table .

 
action_zoom_plus_stroke Semantic engineering menu
Rysunek: Semantic engineering menu

Tabela: Semantic Engineering Menu

Command

Description

Remove from view

Click to remove the selected semantic item from the table. The semantic item remains in the semantic model and keep all its relationship.

Change class

Click to change the class the selected sementic item belongs to.

Clear view

Click to clear the view in the Semeanti engineering table. All semantic items remanins in the semantic model and keep all their relationship.

Set path

Click to open the Select Object and Properties dialog box to create a relationship between the selected semantic object and an EBO object.

Clear path

Click to remove the relationship between the selected semantic item and the EBO object.

Add points

Click to add a semantic point.

Find and replace

Click to open the Find and Replace dialog box.

Remove relation

Click to remove the relationship between the selected semantic item and all other related semantic items.

Copy

Click to copy the semantic item.

Paste

Click to paste a semantic item.

Delete

Click to delete a semantic item.

Navigate to

Click to navigate to the EBO object related to the selected semantic item.

Properties

Click to open the properties for the selected semantic item.

  • Semantic Engineering Overview
  • Semantic Engineering View
  • Semantic Engineering Menu
  • Semantic Engineering Navigation Search Tab
  • Semantic Engineering Navigation Brick Tab
  • Semantic Editing Table
  • Semantic Engineering Context Menu