earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, MP-C, MP-V, AS-P, RP-C, RP-IO , RP-V
功能: SmartX IP Controller 设备
产品版本: 2023, 2024, 7.0
2023/11/27

MS/TP DIP Switches

You must configure the DIP switches as part of the commissioning process for the RP and MP controllers and RP-IO modules that only support MS/TP communications.

有关更多信息,请参阅 BACnet MS/TP Network Communications .

有关更多信息,请参阅 EasyLogic RP-IO .

提示:

Use only switches 1-7. Switch 8 is unused.

See the table and graphic that follows for more information on the switches and their ON values.

表格: DIP Switch ON Values

Switch

ON value

1

1

2

2

3

4

4

8

5

16

6

32

7

64

 
action_zoom_plus_stroke Address DIP switches
图: Address DIP switches

For example, to configure address 6, configure DIP switches 2 and 3 to ON and switches 1, 4, 5, 6 and 7 to OFF.

有关更多信息,请参阅 Configuring the MS/TP Address .

  • EasyLogic RP-IO
  • BACnet MS/TP Network Communications
  • Configuring the MS/TP Address