earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Pojęcie

Pojęcie


Produkty: AS-B, Enterprise Central, Enterprise Server, AS-P
Funkcje: Semantic
Wersja produktu: 2022
2022-03-25

Edit Semantic Items

arrow1_rotationSemantic Labels arrow1_rotationSemantic Relations arrow1_rotationSemantic Paths arrow1_rotationSemantic Class arrow1_rotationUpdating the Semantic Model

You can edit the semantic items in a number of ways.

Semantic Labels

Semantic labels are labels that helps to identify a semantic item. Semantic labels can be edited or removed. Semantic labels can also be replaced using Find and repalce.

Więcej informacji zawiera Adding or Editing a Label of a Semantic Item .

Więcej informacji zawiera Find and Replace Labels and Paths on Semantic Items .

Semantic Relations

Semantic relations are relations between semantic items.

Więcej informacji zawiera Removing a Relation Between Semantic Items .

Semantic Paths

The semantic path defines the relation between a semantic item and an EBO object. Semantic path can be changed or removed. Semantic paths can also be replaced using Find and repalce.

Więcej informacji zawiera Editing the Semantic Path .

Więcej informacji zawiera Find and Replace Labels and Paths on Semantic Items .

Semantic Class

All semantic items are part of a class. You can change the class of a semantic item.

Więcej informacji zawiera Changing the Class of a Semantic Item .

Updating the Semantic Model

Update the semantic model if you have added alarms or trend logs to an EBO object that already have a relation to a semantic item. When you update the semantic model the alarm and trend log is added to the semantic model.

Więcej informacji zawiera Updating the Semantic Model .

  • Semantic Engineering Workflow
  • Opening the Semantic Engineering View
  • Adding or Editing a Label of a Semantic Item
  • Find and Replace Labels and Paths on Semantic Items
  • Removing a Relation Between Semantic Items
  • Editing the Semantic Path
  • Find and Replace Labels and Paths on Semantic Items
  • Changing the Class of a Semantic Item
  • Updating the Semantic Model