earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: AS-B, Enterprise Central, Enterprise Server, AS-P
Funkcje: Semantic
Wersja produktu: 2022
2022-03-25

Updating the Semantic Model

Update the semantic model if you have added alarms or trend logs to an EBO object that already have a relation to a semantic item. When you update the semantic model the alarm and trend log is added to the semantic model.

Pokaż więcej
action_close

Semantic engineering is the process describing an EcoStruxure Building operation database using semantic s .

All engineering regarding semantics is done in WorkStation.

Semantic Engineering Workflow

Use this workflow to make a semantic description of your EcoStruxure Building Operation database.

Więcej informacji zawiera Semantic Engineering Workflow .

To update the semantic model
  • In the Semantic engineering view , in the Semantic engineering menu, click Update semantic model .

  • Opening the Semantic Engineering View
  • Clearing the Semantic Editing Table View
  • Creating Semantic Objects using Drag and Drop
  • Adding a Semantic Item to the Semantic Model
  • Adding a Semantic Point to the Semantic Model
  • Copying and Pasting a Semantic Item
  • Editing the Semantic Path
  • Changing the Class of a Semantic Item
  • Updating the Semantic Model