earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P
Functionalities: Semantic
Product version: 2023
12/17/2022

Auto Generate Semantic Item Workflow

Use the Auto generate semantic items workflow to automatically generate semantic item.

 
action_zoom_plus_stroke Auto generate semantic item workflow
Figure: Auto generate semantic item workflow
Create and import a naming convention

You must start by creating a naming conversion where the object names in EBO get a corresponding semantic type.

For more information, see Creating a Naming Convention .

The naming convention is visible in the Semantic type column after the import.

Auto generate semantic items

You auto generate semantic items to connect the EBO objects with the corresponding semantic item based on the naming convention file.

For more information, see Auto Generating Semantic Items .

Check the result in the semantic engineering workspace

Open the Semantic Engineering workspace to check the result of the auto generating of semantic items.

If you are not satisfied with the result of some of the auto generated semantic items, you can correct them in the Semantic engineering view.

For more information, see Edit Semantic Items .

  • Creating a Naming Convention
  • Naming Convention
  • Semantic Engineering Overview
  • Edit Semantic Items
  • Semantic Engineering Workflow