Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P
Fonctionnalités : Semantic
Version produit : 2024, 7.0
03/12/2024

Creating Semantic Objects using Drag and Drop

You can create a semantic item with a relation to an EBO object using drag and drop.

Afficher plus
action_close

Semantic engineering is the process describing an EcoStruxure Building operation database using semantic s .

All engineering regarding semantics is done in WorkStation.

Semantic Engineering Workflow

Use this workflow to make a semantic description of your EcoStruxure Building Operation database.

Pour plus d'informations, voir Semantic Engineering Workflow .

To create semantic objects using drag and drop
  • From the System Tree pane, drag the EBO object to the Semantic Editing Table .

  • Opening the Semantic Engineering View
  • Clearing the Semantic Editing Table View
  • Creating Semantic Objects using Drag and Drop
  • Adding a Semantic Item to the Semantic Model
  • Adding a Semantic Point to the Semantic Model
  • Copying and Pasting a Semantic Item
  • Editing the Semantic Path
  • Changing the Class of a Semantic Item
  • Updating the Semantic Model