earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: User Management
Product version: 2022, 2023
7/5/2022

User Management Dialog Box – Appearance Tab

Use the Appearance tab to configure user settings such as language, time, and display mode.

 
action_zoom_plus_stroke Appearance tab
Figure: Appearance tab

Table: Appearance Tab

Component

Description

Show invalid objects

Select if the user should be able to see invalid objects. For more information, see Invalid Objects .

Enable session notification

Select if the user should be able to enable session notifications.

Only use classic function block program user

Select if the user only can use classic function block program. For more information, see Graphical Programming .

Language

Select the user’s language. For more information, see Regional Settings .

Date, time and number format

Select the user’s date, time, and number format. For more information, see Regional Settings .

System of measurement

Select the user’s system of measurement. For more information, see Regional Settings .

Decimals

Select the user’s decimals. For more information, see Regional Settings .

Relative time

Select the user’s relative time. For more information, see Regional Settings .

Dark Mode

Select the user’s dark mode. For more information, see Theme Settings .

Size Mode

Select the user’s size mode. For more information, see Theme Settings .

Workspace Mode

Select the user’s workspace.

  • Create and Administer User Accounts in WebStation
  • Theme Settings
  • Regional Settings
  • User Management Dialog Box – Profile Tab
  • User Management Dialog Box – Access Tab