earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : MP-V
Fonctionnalités : Matériel
Version produit : 2022, 2023, 2024, 7.0
17/12/2022

RJ45 Pinout for the RS-485 Port of the MP-V Controller

This section provides the RJ45 pinout for the MP-V controller's RS-485 port.

The RS-485 port is labeled RS-485 Com A. Pour plus d'informations, voir MP-V Communication Ports .

Déclaration

The labeling of the RS-485 port differs between different hardware versions of the MP-V controllers. Pour plus d'informations, voir Differences Between MP-V Hardware Versions .

The wiring recommendations for the RS-485 port depend on the type of network the port is used for. Pour plus d'informations, voir Communication Port Wiring .

 
action_zoom_plus_stroke RJ45 pinout for the MP-V controller RS-485 Com A port
Figure : RJ45 pinout for the MP-V controller RS-485 Com A port

Table : RJ45 Pinout for the MP-V Controller RS-485 Com A Port

RJ45 Pin

Description

1

Not connected

2

TXEN

3

RS485+ (A)

4

+24 VDC

5

Ground

6

RS485– (B)

7

+24 VDC

8

Ground

  • Wiring
  • Communication Port Wiring
  • MP-V Communication Ports
  • MP-V Sensor Bus
  • MP-V BACnet MS/TP Support
  • Differences Between MP-V Hardware Versions
  • MP-V Models