Use the Tenant Repositories dialog box to add and edit tenant repository.
Component |
Description |
|
Add Click to add a tenant repository. For more information, see Tenant Repository . |
|
Edit Click to edit a tenant repository. Click to add a tenant repository. For more information, see Tenant Repository . |
|
Remove Click to remove a tenant repository from the list. For more information, see Tenant Repository . |
Lead object |
Enter the object that acts as the lead for this object. For more information, see Lead and Shadow Relationship . |