earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: Semantic
产品版本: 2023
2023/2/7

Semantic Tenant Repository Workflow

Use this workflow to create and configure tenant repositories.

 
action_zoom_plus_stroke Semantic tenant repository workflow
图: Semantic tenant repository workflow
Set the semantic permissions

Make sure that you have semantic permission.

有关更多信息,请参阅 Configuring Semantic Permissions .

Add and configure a tenant repository on the EcoStruxure Building Operation server

You add a tenant repository in EcoStruxure Building Operation to create a tenant repository on the EcoStruxure Building Operation server define the filter that you want to use on the semantic information and to create a password for the tenant repository.

有关更多信息,请参阅 Adding a Tenant Repository on the EcoStruxure Building Operation Server .

Create tenant repositories on the semantic database

When you have added and configured the tenant repositories on the EcoStruxure Building Operation server you create the repositories on the semantic database. All tenant repositories on the EcoStruxure Building Operation server are created at the same time when you create the tenant repositories on the semantic database.

有关更多信息,请参阅 Creating Tenant Repositories on the Semantic Database .

Populate the tenant repositories

When the semantic configuration is done you upload the semantic data matching the configured filter to the semantic database. Whenever you make any changes to the semantic model on the EcoStruxure Building Operation server you must populate the tenant repositories.

有关更多信息,请参阅 Populating a Tenant Repository .

Connect a user group to the tenant repository

The last step is to connect the EcoStruxure Building Operation to a specific tenant repository.

有关更多信息,请参阅 Connecting a User Group to the Tenant Repository .

  • Semantic Overview
  • Semantic Engineering Overview
  • Semantic Tenant Repository Workflow
  • Tenant Repository
  • Adding a Tenant Repository on the EcoStruxure Building Operation Server
  • Creating Tenant Repositories on the Semantic Database
  • Populating a Tenant Repository
  • Connecting a User Group to the Tenant Repository