earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concetto

Concetto


Prodotti: MP-V, RP-C, RP-V
Funzionalità: Hardware
Versione del prodotto: 2022, 2023, 2024, 7.0
17/12/2022

RS-485 Power Adapter Ports, Terminals, and Switch

The RS-485 Power Adapter is equipped with dual RJ45 ports, a 4-position removable screw terminal block, and a 2-pole slide switch.

 
action_zoom_plus_stroke RJ45 ports, screw terminals, and slide switch
Figura: RJ45 ports, screw terminals, and slide switch
RJ45 ports

The adapter's two RJ45 ports are marked:

  • IN PORT

  • OUT PORT

You use the IN PORT to connect the adapter to an RP or MP controller RS-485 Com (RJ45) port when you want to convert the RJ45 interface to/from screw terminals.

You use both the IN PORT and OUT PORT to connect the adapter to an RS-485 based network with RJ45 interface, such as Room Bus or Sensor Bus, when you want to connect an external 24 VDC power supply to the bus.

Screw terminals

The 4-position removable screw terminal block allows connection either to an RS-485 based network such as a Modbus RTU network or to an external 24 VDC power supply.

Slide switch

The 2-pole slide switch has two positions, which are marked:

  • 24 VDC EXT

  • 24 VDC INT

The switch allows the choice to inject 24 VDC to an RS-485 bus, thereby powering devices connected to the bus. 24 VDC can either be supplied via the adapter from an external 24 VDC power supply or from the RP or MP controller RS-485 Com port.

You move the switch to the EXT (External) position when you want to use an external 24 VDC power supply.

Avviso

It is recommended to move the slide switch on the adapter to the EXT (External) position before connecting the external 24 VDC power supply.

You move the switch to the INT (Internal) position when you want to use the RP or MP controller to supply 24 VDC (3 W or 2 W).

  • RS-485 Adapters
  • RS-485 Power Adapter
  • Convert a BACnet/IP Controller RS-485 Interface
  • Enable Injection of 24 VDC from an External Power Supply to an RS-485 Bus