earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WebStation
功能: 基本功能
产品版本: 2024, 7.0
2024/12/2

Setting a Timeout on a Forced Value WebStation

You set a timeout on a forced value when you want the value to be unforced automatically at a fixed time.

显示更多
action_close

When you force a value, you override all input from the system. For example, if a schedule is set to enable a device at 09:00, but you want to enable it at 08:00, you can force the enablement at 08:00.

You can manually release a forced value at any time or you can automate the release, using a Timed Force utility object to specify the duration or end time of the force. 有关更多信息,请参阅 Timed Force Objects .

When you release a forced value, the value returns to its normal status.

In WorkStation, you can view the unforced value, which is the real value from the system, at any time. 有关更多信息,请参阅 Viewing an Unforced Value .

Timeout on forced values

You can set a timeout on forced values so that the forced value is automatically unforced after a fixed time. The time can be a duration, for example two hours. The forced value can also be unforced at a specific calendar date and time.

有关更多信息,请参阅 Setting a Timeout on a Forced Value .

有关更多信息,请参阅 Setting a Timeout on a Forced Value WebStation .

Indication in WorkStation

A forced value is indicated by orange color in the properties dialog boxes. In in the Watch pane, a forced value is indicated by a pointing hand

 
action_zoom_plus_stroke
.

In the List View and Search View, a forced value is indicated by the text [Forced] in the 'Value' column.

In WorkStation, you can view the unforced value, which is the real value from the system, at any time. 有关更多信息,请参阅 Viewing an Unforced Value .

Indication in WebStation

A forced value is indicated by orange color and a pointing hand in the List view.

Indication in Function Block Graphics Viewer

A forced value is indicated by orange color in Function Block Graphics Viewer. 有关更多信息,请参阅 Forced Value Indication in Function Block Graphics Viewer .

Search for forced values

You can search for forced values using the search function in WorkStation.

有关更多信息,请参阅 Searching for Forced Values .

You can search for forced values in WebStation using Diagnostics.

有关更多信息,请参阅 Displaying a List of Forced Values in WebStation .

To set a timeout on a forced value in WebStation
  1. In Webstation, click the value you want to set a timeout on.

  2. In the value row, click Force .

  3. Click the Set timeout button

     
    action_zoom_plus_stroke
    .

  4. Chose if you want a duration of the forced value or if you want the value to be unforced on specific date and time.

  5. Click OK .

  6. Click Save .

  • Forced Values
  • Forcing a Value
  • Releasing a Forced Value