earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Modalità

Modalità


Prodotti: AS-B, Edge Server, Device Administrator, AS-P
Funzionalità: Hardware, Gestione della licenza
Versione del prodotto: 2023
16/12/2022

Returning Demo Licenses from SpaceLogic Automation Servers

You return demo licenses after they have expired or when you commission a site.

You cannot activate or deactivate licenses when the automation server is connected using a USB cable.

Mostra di più
action_close

Use this workflow to return demo licenses from automation servers.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Return demo licenses from SpaceLogic automation servers workflow
Figura: Return demo licenses from SpaceLogic automation servers workflow
Return demo licenses from automation servers

Return the demo licenses from your automations servers using Device Administrator.

You must return all the demo licenses from the automation servers before you remove the demo license from Device Administrator.

Per maggior informazioni, consulta Removing Demo Licenses File from Device Administrator .

Per maggior informazioni, consulta Returning All Demo Licenses from the Selected SpaceLogic Automation Servers .

Do not remove the demo licenses file from Device Administrator until all demo licenses are removed from your automation servers.

Remove demo licenses file from Device Administrator

When you have returned all demo licenses from your automation server you can remove the demo licenses file from Device Administrator if you are not going to use the demo license again.

Per maggior informazioni, consulta Removing Demo Licenses File from Device Administrator .

To return demo licenses from SpaceLogic automation servers
  1. In Device Administrator, click Servers .

  2. Select Show licenses .

  3. In the Assign Licenses view, in the License status column, click the Show products button

     
    action_zoom_plus_stroke
    .

  4. In the Assign column, in the row for Demo , clear Assign .

  5. In the Deactivate Demo License dialog box, click Yes .

  6. Click OK .

Repeat the procedure for all other automation servers you want to return demo licenses from.

  • Demo Licensing Overview
  • Return Demo Licenses from SpaceLogic Automation Servers Workflow
  • Removing Demo Licenses File from Device Administrator
  • Assign Licenses View