earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Device Administrator, AS-P
Functionalities: License Management
Product version: 2024
12/3/2024

Assigning Demo Licenses on Field Servers

You assign demo licenses to the field servers that you want to use for demo purposes, or when building a site.

You cannot activate or deactivate licenses when the field server is connected using a USB cable.

Show More
action_close

Use this workflow to add and assign a demo license on field servers.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Adding and assigning demo licenses on field servers workflow
Figure: Adding and assigning demo licenses on field servers workflow
Download a demo license file

Download a demo licence file from https://ecoxpert.se.com/. The demo license is called Evaluation license.

Add a demo license to Device Administrator

Add the demo licenses file to Device Administrator.

For more information, see Adding a Demo License File to Device Administrator .

Assign demo licenses on field servers

When the demo licenses file has been added to Device Administrator you can assign demo licenses to field servers.

For more information, see Assigning Demo Licenses on Field Servers .

To assign demo licenses on field servers
  1. In Device Administrator, click Servers .

  2. Select Show licenses .

  3. In the Assign Licenses view, in the License status column, click the Show products button

     
    action_zoom_plus_stroke
    .

  4. In the Assign column, in the row for Demo , select Assign .

  5. In the Activate Demo License dialog box, click Yes .

  6. Click OK .

Repeat the procedure for all other field servers you want to assign demo licenses to.

  • Demo Licensing Overview
  • Adding and Assigning Demo Licenses on Field Servers Workflow
  • Adding a Demo License File to Device Administrator
  • Assign Licenses View