earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: RP-V
Функции: Аппаратное обеспечение
Версия продукта: 2022, 2023, 2024, 7.0
30.03.2023

RJ45 Pinout for the RS-485 Port(s) of the RP-V Controllers

This section provides the RJ45 pinout for the RP-V controllers' RS-485 port(s).

The number of RS-485 ports with RJ45 interface differ between the different controller models.

Regarding the differences in the set of RS-485 ports, the RP-V models can be divided into the following two categories:

  • RP-V-4A and RP-V-5A

  • Model with “-M” in the product name: RP-V-5C-M

Более подробную информацию см. RP-V Models .

The RP-V-4A and RP-V-5A models have two RS-485 ports with RJ45 interface, which are labeled RS-485 Com A and RS-485 Com B. The RJ45 pinout differs only with regards to pin 2 between the two RS-485 ports.

The RP-V-5C-M model has one RS-485 port with RJ45 interface, which is labeled RS-485 Com A. The RJ45 pinout for RS-485 Com A port is the same as for the other RP-V models.

The wiring recommendations for the RS-485 ports depend on the type of network the ports are used for. Более подробную информацию см. Communication Port Wiring .

 
action_zoom_plus_stroke RJ45 pinout for the RS-485 port(s) of the RP-V controllers
Рисунок: RJ45 pinout for the RS-485 port(s) of the RP-V controllers

Таблица: RJ45 Pinout for the RS-485 Com A Port

RJ45 Pin

Description

1

Not connected

2

Not connected

3

RS485+ (A)

4

+24 VDC

5

Ground

6

RS485– (B)

7

+24 VDC

8

Ground

Таблица: RJ45 Pinout for the RS-485 Com B Port

RJ45 Pin

Description

1

Not connected

2

TXEN

3

RS485+ (A)

4

+24 VDC

5

Ground

6

RS485– (B)

7

+24 VDC

8

Ground

  • Wiring
  • Communication Port Wiring
  • RP-V Communication Ports
  • Communication Ports on RP-V-4A and -5A
  • Communication Ports on RP-V-5C-M
  • RP-V Sensor Bus
  • RP-V Room Bus
  • RP-V Modbus
  • RP-V Models