earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Device Administrator, AS-P
Functionalities: Hardware, License Management
Product version: 2023
12/17/2022

Adding an Entitlement without the HTML file when Automation Server is not Connected to License Server (FNO)

You add the entitlement to view the License Products available for activation on automation servers.

Show More
action_close

Device Administrator is used to manage licenses on automation servers.

Software and Features that Require Licenses

A number of software features need licenses.

For more information, see Software and Features that Require Licenses .

Entitlements, Products, and Licenses

Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.

Automation Server Licensing Workflow

Use one of these workflows, depending on if the automation servers are connected or not connected to the Internet.

For more information, see Automation Server Licensing on Automation Servers Connected to Internet Workflow .

For more information, see Automation Server Licensing on Automation Servers not Connected to Internet Workflow .

Certificates

It is recommended to use HTTPS for the communication between Device Administrator and automation servers when you manage licenses.

For more information, see Certificates Managed using Device Administrator .

Return Licenses on SpaceLogic Automation Servers

You can return licenses from automation servers.

For more information, see Return Licenses on SpaceLogic Automation Servers .

To add an entitlement without the HTML file when automation server is not connected to License Server (FNO)
  1. In Device Administrator, click Entitlements .

  2. Click the Add Entitlement down arrow and click Manually .

  3. Enter the entitlement ID.

  4. Click Next .

  5. Click Skip .

    If you know that you do not have any server connected to internet in the list, click Skip . If you do not click Skip , Device Administrator goes through all servers in your list until it finds one that is connected to internet.

  6. In the Entitlement Products - Enter Manually list , enter the Activation ID, Description and seat count for the product.

  7. Click Add Product , to add more products.

  8. Click Add .

When there is no connection between the automation server and License Server, Device Administrator cannot synchronize the number of licenses in the entitlement that are available for activation.

Instead, Device Administrator assumes that all licenses that was purchased can be activated

  • Automation Server Licensing Overview
  • Order Information Request
  • Licenses Activation Server
  • Add and Setup Entitlement
  • Assign Licenses View
  • Assigning Licenses
  • Activating Licenses Online
  • Adding an Entitlement using the HTML file when Automation Server is not Connected to License Server (FNO)
  • Automation Server Licensing on Automation Servers Connected to Internet Workflow
  • Automation Server Licensing on Automation Servers not Connected to Internet Workflow