earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: AS-B, Device Administrator, AS-P
Функции: Аппаратное обеспечение, Управление лицензиями
Версия продукта: 7.0
27.02.2025

Adding an Entitlement using the HTML file when an EcoStruxure BMS Server is Connected to License Activation Server

You add the entitlement to view the License Products available for activation on EcoStruxure BMS servers.

Показать больше
action_close

Device Administrator is used to manage Centralized Licensing on EcoStruxure BMS servers. Centralized Licensing is the main Licensing feature in EcoStruxure Building Operations.

From version 7.0 a new way of licensing is used. Device Administrator is used to handle most of the licenses.

All 7.0 and later EcoStruxure Building Operation BMS servers uses centralized licensing.

All pre 7.0 EcoStruxure Building Operation BMS servers uses the old licensing.

Centralized Licensing Top Server Concept

Central licensing is administered from the top server in the system using Device Administrator. When the top server is added to Device Administrator you can assign and activate all licenses required on your system from Device Administrator.

Более подробную информацию см. Top Server Concept .

Centralized Licensing Workflow

Use this workflow to assign and activate licenses.

Multi-version System

A multi-version system uses both the old, pre 7.0 version, licensing system and Centralized Licensing.

Более подробную информацию см. Multi-version System Licensing .

Upgrading

In a multi-version system running 7.0 and 6.0 and earlier version you must upgrade License Administrator if you want to use the editors and clients. Более подробную информацию см. Editors and Clients That Uses Licenses Administered by License Administrator .

After the upgrade to 7.0 you must install new licenses for all other products and features using Device Administrator.

Software and Features that Require Licenses

A number of software and features need licenses.

Более подробную информацию см. Software and Features that Require Licenses .

Entitlements, Products, and Licenses

Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.

EcoStruxure BMS Centralized Licensing Workflow

Use one of these workflows, depending on if the field servers are connected or not connected to the Internet.

Более подробную информацию см. Centralized Licensing on EcoStruxure BMS Servers Connected to Internet Workflow .

Более подробную информацию см. EcoStruxure BMS Server Licensing on Servers not Connected to Internet Workflow .

Certificates

It is recommended to use HTTPS for the communication between Device Administrator and the EcoStruxure BMS servers when you manage licenses.

Более подробную информацию см. Certificates Managed using Device Administrator .

Return Licenses on Field Servers

You can return licenses from EcoStruxure BMS servers.

Более подробную информацию см. Return Licenses on EcoStruxure BMS Servers .

To add an entitlement using the HTML file when an EcoStruxure BMS server is connected to License Activation Server
  1. In Device Administrator, click Entitlements .

  2. Click Add Entitlement or click from Entitlement Certificate File .

  3. Click Browse and select the HTML entitlement certificate file.

  4. Click Next .

  5. Click Add .

  • Centralized Licensing Overview
  • Order Information Request
  • Licenses Activation Server
  • Add and Setup Entitlement
  • Assign Licenses View
  • Assigning Licenses
  • Activating Licenses Online
  • Adding an Entitlement without the HTML file when an EcoStruxure BMS Server is Connected to License Activation Server
  • Centralized Licensing on EcoStruxure BMS Servers Connected to Internet Workflow
  • EcoStruxure BMS Server Licensing on Servers not Connected to Internet Workflow