earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C
Functionalities: Hardware
Product version: 2023, 2024
3/30/2023

RP-C-16C-F-230V Pluggable Connectors

The RP-C-16C-F-230V controller model has PCB mounted connectors for the power input, the input for an external 24 VAC/VDC power supply, the SSR outputs, and the universal inputs/outputs. The PCB mounted connectors mate with pluggable connectors. The PCB mounted connectors are mechanically keyed and color-coded, which allows the matching external connectors to be plugged in on site quickly and easily.

The pluggable connectors mean time savings and cost reductions for the installation, compared to wiring terminal blocks on site. The connectors can quickly and easily be plugged together on site.

The RP-C-16C-F-230V controller uses 2, 3, or 4 pole connectors for the different inputs and outputs.

The connectors are mechanically keyed, which means the following connections cannot be made:

  • A connector for AC mains cannot be plugged into a connector for low-voltage applications.

  • A connector for low-voltage applications cannot be plugged into a connector for AC mains.

The matching connectors are locked together.

The connectors are also color-coded to help the installers and electricians to choose the correct, matching external connector. The connectors are color-coded:

  • Black: For AC mains (230 VAC) power input.

  • White:

    • For 24 VAC/VDC external power supply input.

    • For SSR outputs with 24 VAC/VDC power distribution.

  • Light blue: For universal inputs/outputs (which are designed for low-voltage applications).

  • Turquoise blue: For configurable I/Os (which can be configured either as SSR outputs or universal inputs/outputs).

 
action_zoom_plus_stroke Color-coded connectors
Figure: Color-coded connectors

The matching external connectors are not provided but need to be ordered separately from Schneider Electric. For more information, see Required External Connectors for the RP-C-16C-F-230V Controller Model .

  • RP-C Controllers
  • RP-C Models
  • Required External Connectors for the RP-C-16C-F-230V Controller Model
  • Plugging an External Connector into an RP Controller Expansion Module or RP-C-16C-F-230V Controller
  • Removing an External Connector from an RP Controller Expansion Module or RP-C-16C-F-230V Controller