The RP controller provides a combination of communication ports, such as:
Ethernet port(s)
USB port(s)
RS-485 port(s)
The number and types of communication ports differ between the different controller models.
Regarding the differences in the set of communcation ports, the RP-C models can be divided into the following three categories:
Models with “-F” in the product name:
RP-C-12A-F-24V, RP-C-12B-F-24V, RP-C-12C-F-24V, RP-C-16A-F-230V, RP-C-16B-F-24V, and RP-C-16B-F-230V
RP-C-16C-F-230V model
Models with “-M” in the product name:
RP-C-12A-M-24V, RP-C-12B-M-24V, and RP-C-16A-M-24V
Per maggior informazioni, consulta RP-C Models .
The RP-C provides the following combination of communication ports:
Two Ethernet ports
Two USB ports
Two RS-485 ports (RJ45)
Per maggior informazioni, consulta Communication Ports on RP-C Models with “-F” in the Product Name .
The RP-C provides the following combination of communication ports:
Two Ethernet ports
One USB port
Three RS-485 ports (RJ45)
Per maggior informazioni, consulta Communication Ports on RP-C-16C-F-230V .
The RP-C provides the following communication ports:
One RS-485 port with RJ45 interface
One RS-485 port with terminal block
Per maggior informazioni, consulta Communication Ports on RP-C Models with “-M” in the Product Name .