earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C
Functionalities: Hardware
Product version: 2023, 2024, 7.0
10/7/2024

Communication Ports on RP-C-16C-F-230V

arrow1_rotationEthernet Ports arrow1_rotationUSB Port arrow1_rotationRS-485 Ports

The RP-C provides the following combination of communication ports:

  • Two Ethernet ports

  • One USB port

  • Three RS-485 ports (RJ45)

Ethernet Ports

The two Ethernet ports are labeled:

  • Ethernet 1

  • Ethernet 2

The two Ethernet ports are 10/100BASE-TX (RJ45) ports. When both Ethernet ports are enabled, they function as an onboard Ethernet switch. Disabling the second Ethernet port disables the switching function. The switching function enables flexible network topologies. For more information, see BACnet/IP Controller Network Topologies . The second port also provides a connection point for a laptop running the Commission mobile application.

For more information, see Communication Port Wiring .

USB Port

The USB port is of the following type:

  • USB host port

The USB host port is a USB 2.0 type-A port, which is rated 2.5 W. The USB host port can be used for connection of Wireless Adapter - Advanced to add Zigbee TM wireless connectivity to the RP-C controller. The adapter can be used to extend the controller's point count and bring flexibility in retrofit applications. For more information, see Wireless Adapter - Advanced .

For more information, see Communication Port Wiring .

RS-485 Ports

The three RS-485 ports are labeled:

  • RS-485 Com A

  • RS-485 Com B

  • RS-485 Com C

The RS-485 Com A, Com B, and Com C ports are rated 3 W (24 VDC).

The three RS-485 ports are RJ45 ports. For more information, see RJ45 Pinout for the RS-485 Port(s) of the RP-C Controllers .

Each port can be configured to use one of the following three communication protocols for different types of networks:

  • Sensor bus

  • Room bus

  • Modbus

Note:

An RP-C can have only one of each network type.

The sensor bus is designed for communication with SpaceLogic Sensor devices. For more information, see RP-C Sensor Bus .

The room bus is designed for communication with RP controller expansion modules for connected room solutions. For more information, see RP-C Room Bus .

The Modbus (RTU) network can be used for communication with the KNX Modbus gateway (RP-C-EXT-KNX) and standard Modbus devices. For more information, see RP-C Modbus .

Default configurations:

  • Sensor bus on the RS-485 Com A port

  • Room bus on the RS-485 Com B port

  • Modbus on the RS-485 Com C port

For more information, see Communication Port Wiring .

  • Hardware Overview
  • RP-C Communication Ports
  • RP-C Controllers
  • BACnet/IP Controller Network Topologies
  • Communication Port Wiring
  • RP-C Sensor Bus
  • RP-C Room Bus
  • RP-C Modbus
  • Wireless Adapter - Advanced
  • KNX Modbus Gateway RP-C-EXT-KNX
  • RJ45 Pinout for the RS-485 Port(s) of the RP-C Controllers