earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C
Functionalities: Hardware
Product version: 2023, 2024, 7.0
3/30/2023

Communication Ports on RP-C Models with “-M” in the Product Name

The RP-C provides the following communication ports:

  • One RS-485 port with RJ45 interface

  • One RS-485 port with terminal block

This applies to the following RP-C models with “-M” in the product name:

  • RP-C-12A-M-24V, RP-C-12B-M-24V, and RP-C-16A-M-24V

RS-485 Port with RJ45 Interface

The RS-485 port is labeled:

  • RS-485 Com A

The RS-485 Com A port is rated 3 W (24 VDC).

The RS-485 Com A port is an RJ45 port. For more information, see RJ45 Pinout for the RS-485 Port(s) of the RP-C Controllers .

The RS-485 Com A port can be configured to use one of the following two communication protocols for different types of networks:

  • Sensor bus

  • Modbus

Note:

An RP-C can have only one of each network type.

The sensor bus is designed for communication with SpaceLogic Sensor devices. For more information, see RP-C Sensor Bus .

The Modbus (RTU) network can be used for communication with standard Modbus devices. For more information, see RP-C Modbus .

Default configuration:

  • Sensor bus on the RS-485 Com A port

For more information, see Communication Port Wiring .

For more information, see Allocating Flexible Ports .

RS-485 Port with Terminal Block

The RS-485 port with screw terminal block is used for connection to the BACnet MS/TP (RS-485) network.

The screw terminals are labeled:

  • RS-485+

  • RS-485–

  • Shield

For more information, see RP-C-12A-M-24V Screw Terminals .

For more information, see RP-C-12B-M-24V Screw Terminals .

For more information, see RP-C-16A-M-24V Screw Terminals .

For more information, see RS-485 Communications .

  • Hardware Overview
  • RP-C Communication Ports
  • RP-C Controllers
  • RP-C Sensor Bus
  • RP-C Modbus
  • RJ45 Pinout for the RS-485 Port(s) of the RP-C Controllers
  • Allocating Flexible Ports
  • RP-C-12A-M-24V Screw Terminals
  • RP-C-12B-M-24V Screw Terminals
  • RP-C-16A-M-24V Screw Terminals
  • RS-485 Communications