The RP controller provides a combination of communication ports, such as:
Ethernet port(s)
USB port(s)
RS-485 port(s)
The number and types of communication ports differ between the different controller models.
Regarding the differences in the set of communcation ports, the RP-V models can be divided into the following two categories:
RP-V-4A and RP-V-5A
Model with “-M” in the product name: RP-V-5C-M
Pour plus d'informations, voir RP-V Models .
The RP-V-4A and RP-V-5A models provide the following combination of communication ports:
Two Ethernet ports
One USB port
Two RS-485 ports (RJ45)
Pour plus d'informations, voir Communication Ports on RP-V-4A and -5A .
The RP-V-5C-M model provides the following communication ports:
One RS-485 port with RJ45 interface
One RS-485 port with terminal block
Pour plus d'informations, voir Communication Ports on RP-V-5C-M .