earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-IO
Functionalities: Hardware
Product version: 2023, 2024
3/30/2023

RP-IO Module Communication Port

The RP-IO module provides the following communication port:

  • One RS-485 port with terminal block

The RS-485 port with screw terminal block is used for connection to the BACnet MS/TP (RS-485) network.

The screw terminals are labeled:

  • RS-485+

  • RS-485–

  • Shield

For more information, see RP-IO-12A-M-24V Screw Terminals .

For more information, see RP-IO-16E-M-24V Screw Terminals .

For more information, see RS-485 Communications .

  • Hardware Overview
  • RP-C Controllers
  • RP-IO-12A-M-24V Screw Terminals
  • RP-IO-16E-M-24V Screw Terminals
  • RS-485 Communications