earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: Operator Display
功能: 趋势
产品版本: 3.3, 2022, 2023, 2024, 7.0
2023/4/24

Trend Logs Information Screen

Use the trend logs information screen to display the properties recorded for each trend log.

 
action_zoom_plus_stroke Trend logs information screen
图: Trend logs information screen

表格: Trend Logs Information Screen

Component

Description

Log Name

Displays the name of the log that is connected to the trend log list.

Log Unit

Displays the unit of the recorded values.

Start Time

Displays the time of the first record in the trend log list.

Stop Time

Displays the time of the last record in the trend log list.

Hightest Value

Displays the highest calculated value in the trend log list, based on the sample displayed in the screen.

Lowest Value

Displays the lowest calculated value in the trend log list, based on the sample displayed in the screen.

Average

Displays the average value of the trend log list, based on the sample displayed in the screen.

Record Count

Displays the number of records currently residing in the log buffer.

Total Record Count

Displays the total number of records collected in the trend log since its creation.

Log Enable

Displays whether events are logged and data is collected.

Log Interval (in Centisecond)

Displays the time interval in hundredths of seconds between each log recording.

Logging Type

Displays the type of data recorded in the trend log list.

Stop When Full

Displays whether the trend log collects records using polling, Change of Value (COV) or triggered acquisition.

Buffer Size

Displays the maximum number of recordings permitted in the trend log list.

Log Device Object Property

Displays the Device Identifier, Object Identifier, and Property Identifier of the property to be trend logged.

Log Device Object Units

Displays the measuring unit of the property to be trend logged.

  • Trends Handling
  • Trend Logs Screen
  • Trend Logs View Screen
  • Trend Logs Information Screen